Source Control > Show Differences command

Choose this command to initiate a compare operation (using the
Logix Designer
Compare Tool) between the open project and the latest version of the associated file that is found under source control.
Note that this menu item displays only if all of the following conditions exist:
  • an open project exists
  • either the
    Logix Designer
    application has automatically drawn an association between the open project and one under source control, or you have explicitly established that association;
  • the open project is checked out, the check out belongs to the current user, and the path to the open project matches the checked out path recorded by the source control server.
  • a supported version of the
    Logix Designer
    Compare Tool is installed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.