- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Specifying configurations
To specify a configuration:
- Select theConfigurationtab.
- For any changes to take effect, selectOKorApply.In this field:Specify:PID equationSelect independent gains or dependent gains (.PE).Use independent when you want the three gains (P, I, and D) to operate independently. Use dependent when you want an overall controller gain that affects all three terms (P, I, and D).Control actionSelect either E=PV-SP or E=SP-PV for the control action (.CA).Derivative ofSelect PV or error (.DOE).Use the derivative of PV to eliminate output spikes resulting from setpoint changes. Use the derivative of error for fast responses to setpoint changes when the algorithm can tolerate overshoots.Loop update timeEnter the update time (.UPD) for the instruction (greater than or equal to 0).CV high limitEnter a high limit for the control variable (.MAXO).CV low limitEnter a low limit for the control variable (.MINO).Deadband valueEnter a deadband value (.DB).No derivative smoothingEnable or disable this selection (.NDF).No bias calculationEnable or disable this selection (.NOBC).No zero crossing in deadbandEnable or disable this selection (.NOZC).PV trackingEnable or disable this selection (.PVT).Cascade loopEnable or disable this selection (.CL).Cascade typeIf cascade loop is enabled, select either slave or master (.CT).
Provide Feedback