Import > Component command
Choose this command to import the selected Add-On Instruction, data type,
Equipment Phase
, Equipment Sequence
, program routine, string types or trend.This command is not available online, a state in which a device is in direct communication (for example, when
Logix Designer
is monitoring the program file in a controller).Provide Feedback