Failed to modify the properties for the routine <Routine Name>
Attempted to change a property of a routine within the Routine Properties dialog box, but the operation did not succeed. Possible causes are:
- The name is invalid
- The routine was deleted
- The program the routine is contained in was deleted
- Not enough memory
Provide Feedback