Guardmaster 440C-CR30 safety relay configures through Connected Components Workbench software
MILWAUKEE, April 3, 2014 — Machine builders can now easily implement required safety functions while improving productivity with the Allen-Bradley Guardmaster 440C‑CR30 safety relay from Rockwell Automation.
“Machine builders across all industries are seeking safety solutions that go beyond meeting compliance requirements to helping significantly increase both configuration and operation productivity,” said Thomas Helpenstein, product manager, Rockwell Automation. “The flexible, compact Guardmaster 440C‑CR30 safety relay configured via Connected Components Workbench software meets their needs for improved safety, uptime and productivity.”Users can program the safety relay through the free Connected Components Workbench software from Rockwell Automation. Connected Components Workbench software reduces programming time and helps increase productivity by allowing users to create, control and monitor a safety system in the same software environment as their standard control. The Guardmaster 440C-CR30 safety relay meets PLe, SIL 3 per EN ISO 13849-1 and IEC 62061. It is ideal for applications requiring four to nine safety circuits and control of up to five zones.
The distinct graphical user interface and drag-and-drop capabilities of the software help guide users through a simple process of selecting certified safety function blocks for the safety relay. Once programmed, an embedded Modbus interface allows the safety relay to easily communicate diagnostic data to Allen‑Bradley Micro800 controllers, Allen-Bradley PanelView graphic terminals or Allen‑Bradley CompactLogix controllers. Leveraging the embedded communication capabilities and the software allows users to easily monitor, troubleshoot and quickly modify their applications, including performing partial or conditioned shutdowns, as needed. Five status and 16 user-configurable LEDs on the safety relay’s faceplate provide local diagnostics to further aid in status reporting and troubleshooting.
With 22 on-board safety I/O points, including six configurable I/O, the Guardmaster 440C‑CR30 safety relay is the ideal solution for applications requiring multiple safety zones. Without growing the footprint, the safety relay also can be expanded with two standard Micro800 plug-in modules to support 16 additional standard I/O points, saving valuable safety I/O points for user safety systems. The safety relay also permits interoperation with multiple standard-control platforms, enabling the safety control to remain the same even if the standard control changes.
News Release Assets
Image available upon request or at box.net.
About Rockwell Automation About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 22,000 people serving customers in more than 80 countries.
Media Contacts
tmbissel@ra.rockwell.com
beatrice.zvosec@padillacrt.com
Allen-Bradley, CompactLogix, Connected Components Workbench, Guardmaster, LISTEN. THINK. SOLVE., Micro800 and PanelView are trademarks of Rockwell Automation Inc.
Published April 2, 2014