DC motor systems can be upgraded with a reduced number of external devices
MILWAUKEE — The new Allen-Bradley PowerFlex DC field controller from Rockwell Automation enables customers to upgrade their DC motor application to a modern system, without the need for complex external devices. An up-to-date digital networked control system helps customers gather and leverage vital information throughout their enterprise.
The DC field controller provides three-phase, four-quadrant (reversing) DC motor or generator field control. The field controller can be used on its own or with a PowerFlex DC digital drive. In stand-alone mode, it provides power to a DC motor field with a fixed reference by using fixed I/O. The field controller can also control electromagnets and other non-motor loads.
“For DC retrofit applications that require motor reversing, the PowerFlex DC field controller helps eliminate the need for an additional armature bridge or a complex system of external devices, saving customers both time and money,” said Nancy Rivard, product manager for Rockwell Automation. “Having a single source for all automation equipment – including both AC and DC drives – also simplifies machine startup, operation and maintenance.”
Click to download image.
The field controller offers output ratings from 17 amps to 575 amps and input of 200-volts and 500-volts. It enhances the capability of the PowerFlex DC drive family, designed for demanding stand-alone and coordinated drive system applications. The PowerFlex DC drive family is well suited for DC motor applications and retrofits up to 6,000 Hp or 4000 kW.
The PowerFlex DC family has core capabilities aligned with the PowerFlex AC family of drives, including seamless integration into a Logix-based environment, flexible feedback and communication options, as well as voltage settings designed to global standards.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.
Media Contacts
Julie Weber
Rockwell Automation
262.512.2369
jweber2@ra.rockwell.com
Beatrice Zvosec
Padilla
612.455.1914
beatrice.zvosec@padillaco.com
Allen-Bradley, PanelView and Studio 5000 are trademarks of Rockwell Automation Inc.
Published July 2, 2018