Manufacturers seeking to virtualize smaller applications now have a solution that is sized for them. The new VersaVirtual appliance from Rockwell Automation provides all the computing, networking and storage capabilities needed to deploy and maintain up to 15 virtual machines in one ready-to-use appliance.
The VersaVirtual appliance helps save time and money when virtualizing applications in two key ways.
Click to download image.
First, it avoids the potential pitfalls of a do-it-yourself virtualized architecture. Homegrown solutions can take weeks to deploy and require working with multiple vendors. The pre-engineered VersaVirtual appliance arrives at a user’s location preconfigured, where it can be deployed in mere hours. And instead of dealing with multiple vendors, VersaVirtual appliance users have one number to call for support.
Second, the VersaVirtual appliance provides similar capabilities as an Industrial Data Center but with scaled down cost and complexity for smaller applications. This can break down barriers to virtualization for companies that are challenged by solution complexity, lack of skills or resources, and infrastructure costs.
The VersaVirtual appliance comes with one-year remote monitoring and administration so that users receive around-the-clock system monitoring to help prevent downtime. Customers will also receive support from certified IT/OT professionals who have an average response time of three minutes to help resolve technical issues.
Published July 10, 2019