Rockwell Automation expands modular MES offerings
MILWAUKEE — New and expanded applications from Rockwell Automation help reduce the cost and time-to-value of a manufacturing execution system (MES). An MES allows companies to connect, manage, validate and optimize production to help achieve smart manufacturing. However, a traditional MES is cost-prohibitive for many manufacturers.
Now, manufacturers can tap into scalable FactoryTalk ProductionCentre MES applications from Rockwell Automation that address specific manufacturing challenges, like quality, machine performance, track/trace and genealogy. Solutions can start at the machine or work-area level with a single application and with minimal infrastructure requirements, and scale to an integrated MES solution as ROI is realized.
Rockwell Automation has released the following applications, with more to come in the future:
FactoryTalk Production Application – Manufacturers are challenged to optimize production processes, lower structured costs, improve productivity and achieve a near zero-inventory system. The FactoryTalk Production application is a scalable MES solution that addresses the challenges associated with enforcing processes in manufacturing. This application integrates with ERP, and tracks the order and recipe parameters necessary for production. The Production application supports end-to-end production management within a facility, offering a vital platform for continuous improvement.
FactoryTalk Quality Application – Facilities relying on disparate systems and antiquated paper processes cannot guarantee consistent production quality. The newly expanded Quality application allows manufacturers to easily and efficiently model and enforce their plant’s in-process quality regimens at a scalable rate. The application supports a facility’s efforts to deliver a timely, quality product and react quickly to quality issues. Manufacturers can use the Quality application on a project basis and scale up when value is proven. The application can be expanded to include other functionality within the FactoryTalk ProductionCentre MES system or run as a standalone.
FactoryTalk Performance Application – Manufacturing companies today lack visibility into real-time production performance and productivity data. Performance is a modular application that assists manufacturing companies with factory efficiency and production improvement. By providing visibility into the operations performance, this application allows for lean and continuous improvement, preventive manufacturing, improved asset utilization and operational intelligence.
Each expanded MES application is implemented on thin clients for a modern user experience and reduced, IT infrastructure cost. Users can add on each application to their current framework, helping protect their current investments while realizing these additional benefits.
Rockwell Automation has long recognized the importance of connecting independent automation systems in production environments. This modular framework will continue to be built out with applications for warehouse management and process integration throughout 2017.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.
Media Contacts
Paula Puess
Rockwell Automation
440.646.3806
pdpuess@ra.rockwell.com
Laura Landvik
PadillaCRT
612.455.1763
laura.landvik@padillacrt.com
FactoryTalk and ProductionCentre are trademarks of Rockwell Automation Inc.
MILWAUKEE — New and expanded applications from Rockwell Automation help reduce the cost and time-to-value of a manufacturing execution system (MES). An MES allows companies to connect, manage, validate and optimize production to help achieve smart manufacturing. However, a traditional MES is cost-prohibitive for many manufacturers.
Now, manufacturers can tap into scalable FactoryTalk ProductionCentre MES applications from Rockwell Automation that address specific manufacturing challenges, like quality, machine performance, track/trace and genealogy. Solutions can start at the machine or work-area level with a single application and with minimal infrastructure requirements, and scale to an integrated MES solution as ROI is realized.
Rockwell Automation has released the following applications, with more to come in the future:
FactoryTalk Production Application – Manufacturers are challenged to optimize production processes, lower structured costs, improve productivity and achieve a near zero-inventory system. The FactoryTalk Production application is a scalable MES solution that addresses the challenges associated with enforcing processes in manufacturing. This application integrates with ERP, and tracks the order and recipe parameters necessary for production. The Production application supports end-to-end production management within a facility, offering a vital platform for continuous improvement.
FactoryTalk Quality Application – Facilities relying on disparate systems and antiquated paper processes cannot guarantee consistent production quality. The newly expanded Quality application allows manufacturers to easily and efficiently model and enforce their plant’s in-process quality regimens at a scalable rate. The application supports a facility’s efforts to deliver a timely, quality product and react quickly to quality issues. Manufacturers can use the Quality application on a project basis and scale up when value is proven. The application can be expanded to include other functionality within the FactoryTalk ProductionCentre MES system or run as a standalone.
FactoryTalk Performance Application – Manufacturing companies today lack visibility into real-time production performance and productivity data. Performance is a modular application that assists manufacturing companies with factory efficiency and production improvement. By providing visibility into the operations performance, this application allows for lean and continuous improvement, preventive manufacturing, improved asset utilization and operational intelligence.
Each expanded MES application is implemented on thin clients for a modern user experience and reduced, IT infrastructure cost. Users can add on each application to their current framework, helping protect their current investments while realizing these additional benefits.
Rockwell Automation has long recognized the importance of connecting independent automation systems in production environments. This modular framework will continue to be built out with applications for warehouse management and process integration throughout 2017.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.
Media Contacts
Paula Puess
Rockwell Automation
440.646.3806
pdpuess@ra.rockwell.com
Laura Landvik
PadillaCRT
612.455.1763
laura.landvik@padillacrt.com
FactoryTalk and ProductionCentre are trademarks of Rockwell Automation Inc.
Published October 10, 2016