Install FTASecurity Provider

Install FTASecurity Provider

Analytics Security Provider service (called FTASecurity hereafter) provides single sign-on (SSO) support for all of the FactoryTalk® Analytics™ applications including DataView.
  1. Follow the
    4.00.00_Analytics Security Provider Installation Guide (Windows)
    to install FTASecurity.
    NOTE:
    If the FTASecurity Provider is already installed with other FTA Application, it is recommended to use the existing FTASecurity.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.