Execute Database Scripts

Execute Database Scripts

  1. Right-click on the newly created database and select the Query Tool option.
    Query Tool
  2. Maximize the pgAdmin4 window.
  3. Click the Folder icon on the tool bar.
    Folder
  4. Switch the Format field to “All Files” and go to the DataView install folder.
    Select File Format
  5. In the Select File dialog open the
    dbscripts
    folder in the
    <DataView_HOME>\FTADataView\dbscripts
    directory.
    IMPORTANT:
    If the files are extracted to a different folder other than the folder shown below, the folder/path instructions may be different for the machine.
    Example:
    <DataView_HOME>\FTADataView\dbscripts\
    DB Script Folder
  6. Select the
    DataViewMainScript.sql
    file and click [Select].
    Database Script - DataViewMainScript
  7. The script is displayed under FTADataView database. Click the [] icon to execute the DataViewMainScript.
    Run the DataViewMainScript
  8. Refresh the database. The new triggers and tables will be added to this database. Refer the following screenshot:
    New Triggers and Tables
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.