Install New Release of DataView

Install New Release of DataView

  1. Follow the steps in Extract DataView Application to extract new release of DataView and Zip files. Extract the new release of DataView files in a new folder.
    Example
    : If the current DataView was installed under
    C:\Rockwell\DataView4.00.00
    , then the new release of DataView should be extracted under
    C:\Rockwell\DataView4.00.01
    .
    TIP:
    This document will refer to %NEW_DATAVIEW_HOME% as the new DataView release installed folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.