Back up

Back up

IMPORTANT:
If the files are extracted to a different folder other than the folder shown below, the folder/path instructions may be different.
  1. Create a backup folder and take backup of the
    application.properties
    file, which is available in the
    <DataView_HOME>\FTADataView\dataview\config
    folder.
  2. Create a backup folder and take backup of the
    dataimporter.properties
    file, which is available in the
    <DataView_HOME>\FTADataView\dataimporter\config
    folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.