Update Enterprise
NOTE:
Only admin users can update the Enterprise details.
Perform the following steps to update the Enterprise details:
- On the left panel, click [Administration], the Enterprise details displays.
- Click the Edit [
] icon on the particular section that you want to edit or update.
- Update the editable fields and click [Save].Enterprise Update
Provide Feedback