Delete Project
NOTE:
You can delete the Project in both list view and detail view.
Perform the following steps to delete the Project:
- Select the checkboxes of the Project(s) that you want to delete.
- Click the [
] icon on the top right corner and click [Delete].
Delete Project - The ‘Delete Project(s)’ dialog displays, click [Delete].Confirm Delete Project
- The “Project(s) are deleted successfully” message displays and the Project is deleted from the list.
Provide Feedback