Create User
Perform the following steps to create an User:
- Click the Administration [
] icon on the top right corner and select the Users tab.
- Click the Add [+] icon.Add User
- In the Identity section, provide the user-specific details.
- Select the Role you want to assign to the user from the drop-down list.
- Click [Add].Add User Cont..
- The “User has been added” message displays and User gets added to the users list.
- You can click on any of the users in the list view to view the details of that user.
Provide Feedback