Deactivate Edge Node
Perform the following steps to Deactivate the Edge Node(s):
- Click [Edge Nodes] on the left navigation panel, the Edge Nodes list view displays.
- Select the checkboxes of the Edge Node(s) that you want to Deactivate.
- Click the [
] icon on the top right corner and click [Deactivate].
Deactivate Edge Node - The ‘Deactivate Edge Node(s)’ dialog displays, click [Deactivate].Deactivate Edge NodeA success message displays as shown below:Confirm DeactivateNOTE:The Deactivated the edge node(s) shows Admin Status as ‘Inactive’ and Run state as ‘Unprovisioned’.
Provide Feedback