Delete Edge Node
The 'Delete' operation removes the edge node(s).
Perform the following steps to Delete the Edge Node(s):
- Click [Edge Nodes] on the left navigation panel, the Edge Nodes list view displays.
- Select the checkboxes of the Edge Node(s) that you want to Delete.
- Click the [
] icon on the top right corner and click [Delete].
Delete Edge Node - The ‘Delete Edge Node(s)’ dialog displays, click [Delete].Delete Edge NodeA success message displays and the selected edge nodes are deleted.
Provide Feedback