Prepare Poweroff
This feature is useful when you need to gracefully shut down the set of applications running on Edge Operating System (Edge OS).
Perform the following steps to Prepare Poweroff of Edge Node(s):
- Click [Edge Nodes] on the left navigation panel, the Edge Nodes list view displays.
- Select the checkboxes of the Edge Node(s) that you want to Power Off.
- Click the [
] icon on the top right corner and click [Prepare Poweroff].
Poweroff Edge Node - The ‘Prepare Poweroff for Edge Node(s)’ dialog displays, click [Prepare Poweroff].Confirm OffboardA success message displays and the selected edge nodes are powered off.
Provide Feedback