Reboot
Perform the following steps to Reboot the Edge Node(s):
- Click [Edge Nodes] on the left navigation panel, the Edge Nodes list view displays.
- Select the checkboxes of the Edge Node(s) that you want to Reboot.
- Click the [
] icon on the top right corner and click [Reboot].
Reboot Edge Node - The ‘Reboot Edge Node(s)’ dialog displays, click [Reboot].Confirm RebootA success message displays as shown below:Reboot Successful
Provide Feedback