Update Edge Operating System (Edge OS) Image
NOTE:
The [
] icon against the edge node indicates that a particular edge node runs the latest version in the edge node list view and you need not to update the latest version of the Edge Operating System (Edge OS).
![](/content/dam/dita/en/factorytalk-edge-manager/v1-00/user-manual/edge-node-management/eve-updated.png/_jcr_content/renditions/original)
Perform the following steps to Update Edge Operating System (Edge OS) Image on Edge Node(s):
- Click [Edge Nodes] on the left navigation panel, the Edge Nodes list view displays.
- Select the checkboxes of the Edge Node(s) that you want to update.
- Click the [
] icon on the top right corner and click [Update EVE-OS Image].
Update EVE Image - The ‘Update EVE Image’ dialog displays, click [Update & Activate].Confirm UpdateA success message displays as shown below:EVE Image Updated
Provide Feedback