View type instances

View instances of a type, such as a window, to view all instances in the information model where the type exists.
  1. In
    Project view
    , navigate to and right-click the type and then select
    Show Instances
    .
  2. In
    Instances of (name)
    , select an instance of the type and select
    Go to ...
FactoryTalk Optix Studio
navigates to the instance of the type. Objects referenced in a NetLogic are not shown.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.