- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create an object from a type
Create an object from a type. The new object instance is automatically of the same type.
- FromType view, double-click the folder with the category of objects.
- Drag the object type into a folder or object inProject view.
The new object appears in
Project view
.Provide Feedback