Create an OPC UA server

Create an OPC UA server that pushes translations from the Server project and populates the Client project with them.
  1. In
    Project view
    , right-click the
    OPC-UA
    folder and select
    New
    OPC UA Server
    .
  2. In
    Properties
    , take a note of the
    Endpoint URL
    property value.
    NOTE: You need the
    Endpoint URL
    property value to configure the OPC UA Client later on.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.