Create project variables

Create the Speed and Acceleration variables to use them in the UI design.
  1. In
    Project view
    , create two variables by right-clicking the
    Model
    folder, and selecting
    New
    Variable
    .
  2. Rename the variables by hovering-over each variable, selecting
    Edit
    , and entering:
    • Speed
    • Acceleration
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.