Implement the main panel

Create a dynamic link to the main panel in the dynamic panel.
  1. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Containers
    Panel loader
    .
  2. Hover-over the panel loader, select
    Edit
    , and enter
    DynamicPanelLoader
    .
  3. In
    Properties
    , create a dynamic link between
    Panel
    and
    ProjectName
    UI
    RemotePanels
    MainPanel (type)
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.