Error - File with same name exists

A writable instance of the file is open in another instance of the
Logix Designer
application. The file was not checked out.
Option
Description
OK
Return to the
Open/Import Project
dialog box
Help
Help about this error
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.