Current Reference page

Use the settings on the
Current Reference
page in the
Axis Properties
dialog box to configure the low pass filter bandwidth and the notch filter frequency for a converter.
The
Current Reference
page is available when, on the
General
page, the
Axis Configuration
is set to
Regenerative AC/DC Converter
or
Low Harmonic AC/DC Converter
.
TIP: To open the Current Reference page:
  1. In the
    Controller Organizer
    , expand the
    Motion Groups
    folder, and double-click an axis.
  2. From the
    Axis Properties
    dialog box, in
    Categories
    , click
    General
    .
  3. In the
    Axis Configuration
    box, select
    Regenerative AC/DC Converter
    or
    Low Harmonic AC/DC Converter
    .
  4. In
    Categories
    , click
    Current Reference
    .
The parameters are unavailable when in online mode and when the axis is
Servo On
.
Parameter
Description
Low Pass Filter Bandwidth
Specifies the break frequency for the low pass filter applied to the active current reference signal.
The default is 0.0 Hertz.
Notch Filter Frequency
Specifies the center frequency of the notch filter applied to the active current reference signal.
The default is 0.0 Hertz.
Parameters
Opens the
Master Axis Parameters
page to configure additional current reference parameters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.