Configure a Power-Up Handler program

Configure a Power-Up Handler program

Configure a program as the Power-Up Handler program. This program is executed on startup after losing power abnormally in Run mode.
IMPORTANT:
The program cannot be scheduled under a task.
To configure a Power-Up Handler program
  1. From the
    Edit
    menu, choose
    Controller Properties
    .
  2. Select the
    Advanced
    tab.
  3. From the
    Power-Up Handler Program
    menu, choose the program to use.
    Note that a program must already exist in the
    Controller Organizer Power-Up Handler
    folder in order for it to be available from this menu.
  4. Select
    OK
    .
Routines in the Power-Up Handler program should perform any startup logic required to reset the system to a useful state after a power loss.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal