Controller Properties dialog box - Minor Faults tab

Use the
Minor Faults
tab on the
Controller Properties
dialog box to display information about the minor faults in the controller.
TIP: To open the Controller Properties dialog box - Minor Faults tab:
  1. On the
    Online
    toolbar, click the
    Controller Properties
    icon.
  2. On the
    Controller Properties
    dialog box, click the
    Minor Faults
    tab.
TIP:
This tab also appears in the
Connected
dialog box to view and clear minor faults without having to correlate with the controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.