Sheet Number

Indicates the sheet number of the sheet you are currently viewing in the function block routine. In addition, this control indicates the total number of sheets in the current function block routine.
Clicking on the pull-down menu allows you to select a specific sheet to view.
TIP:
You can also type a sheet number directly into the sheet number field, and press Enter to navigate directly to that sheet.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.