Project Documentation Language dialog box overview
Use the
Project Documentation Language
dialog box to turn on the Project Documentation Languages feature by selecting a current language for the project.Read the message to understand what effect enabling Project Documentation Languages has on the project.
These are the parameters for the Project Documentation Language dialog box:
- Associate Existing Project Documentation With. A list of all possible languages with which to associate existing project documentation.Tip:There is no specific language selected by default. You can select a language to associate existing documentation with a language.
- Customs. Click to open the Custom Language Configuration dialog box to manage the customized languages in the project.
Provide Feedback