Overview
This course introduces the FactoryTalk® Analytics platform and focuses on FactoryTalk® Analytics™ DataView components.
The FactoryTalk Analytics DataView offering is a self-service data analytics platform, which allows users to generate business insights across multiple data sources. It is designed for manufacturing environments by focusing on industrial connectivity with an intuitive interface with interactive storyboards that allow users to ingest, view, and perform analytics.
DISCLAIMER: This is not the full version of the course. We will be adding lessons in the future that align with the release of FactoryTalk Analytics DataView version 4.0. These lessons will highlight the major functionality and UI changes coming in the next major release.