A Technically Complex Sustainability Solution
When hoisting a load up a mine shaft, electric motors consume energy. But when travelling downwards, they have the potential to become generators.
“Most mine hoists use a brake resistor pack with a cooling fan to deal with the heat generated. But these packs create a single point of failure, and are application-specific, so they need recalculation if a variation in brake power is required,” explained Bell.
“Instead, we proposed for the generating power to be supplied back onto the incoming supply bus, to be absorbed by system loads,” he added.
To make this solution a reality, Rockwell Automation provided Active-Front-End (AFE) Powerflex® 755TR regenerative variable speed drives, low voltage motor control centres, GuardLogix® controllers, ThinManager® software for application management, FactoryTalk® View Site Edition software for a complete real-time overview of HMI operations, network and security services, and product and technical support.
The battery selected to store regenerative energy was a Cat PGS 1260 Battery Energy Storage System (BESS), supplied by EPSA, which provided added redundancy through its parallel inverter and battery stack architecture.
“We have one operational project where we have implemented this solution with two hoist drives, and we are looking into incorporating this into future projects. We also see potential for this solution to be rolled out on new and existing mine shafts internationally,” said Bell.