Loading
Press Release | December 12, 2024

Rockwell’s Medium-Voltage Drive Technology Helps West Fraser Reduce Annual Energy Bill

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
  • West Fraser logo
    Through deployment of a complete Intelligent Packaged Power (IPP) solution from Rockwell, West Fraser is inching closer to its carbon-reduction targets, gaining enhanced operator insights, and enjoying greater asset resilience.

Industrial applications that run things like pumps, fans, conveyors, and compressors are responsible for more than 50%

of the world’s total electricity consumption. One option to dramatically reduce that drag on resources is variable frequency drives (VFDs). These devices can adjust the frequency and voltage of the power supply, which can help improve the motor’s efficiency and even extend the life of the motor.

Rockwell Automation helped West Fraser

, a diversified wood products company, make significant gains towards energy saving targets through an Intelligent Packaged Power
(IPP) solution featuring VFDs. An IPP solution simplifies the integration between process and electrical systems—giving workers immediate access to real-time data on the equipment and how it is operating so they can make better decisions faster.

West Fraser’s plant in Cowie, Scotland, began using a CENTERLINE® 1500

medium-voltage motor control center (MCC) and three PowerFlex® 6000T
medium-voltage VFDs across three of the site’s energy-intensive fan applications. As a result of reducing motor speed by 25%, West Fraser lowered the motor’s energy consumption by approximately 60%, translating into an annual savings of more than $266,000.

This is just one example of how VFDs can have a profound, positive impact in reducing energy consumption and cutting carbon levels.

Published December 12, 2024

 
 

About Rockwell Automation

Rockwell Automation, Inc. (NYSE: ROK), is a global leader in industrial automation and digital transformation. We connect the imaginations of people with the potential of technology to expand what is humanly possible, making the world more productive and more sustainable. Headquartered in Milwaukee, Wisconsin, Rockwell Automation employs approximately 27,000 problem solvers dedicated to our customers in more than 100 countries as of fiscal year end 2024. To learn more about how we are bringing the Connected Enterprise to life across industrial enterprises, visit www.rockwellautomation.com.

About the Rockwell Automation PartnerNetwork

Rockwell Automation believes we're better together—and we do our part by delivering an expansive, global partner ecosystem of market-leading technology, superior support and services, and an integrated and streamlined approach to business. Succeed on an international scale by utilizing our network's breadth of innovative technologies and services that no single vendor can provide alone. To learn more about how the PartnerNetwork is helping to deliver the value of The Connected Enterprise, visit PartnerNetwork Program.


  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Press Releases Chevron RightChevron Right
  5. Chevron LeftChevron Left Rockwell’s Medium-Voltage Drive Technology Helps West Fraser Reduce Annual Energy Bill Chevron RightChevron Right
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
You can update your preferences at any time. For more information please see our Privacy Policy
CloseClose