By HMS Networks
Remote access provides the ability to remotely connect to intelligent devices such as programmable logic controllers (PLCs), human-machine interfaces (HMls) or robots, with similar functionality as if being on-site with those devices. The resulting cost savings, and ability to act immediately when a machine fails, verifies that machines are working at their maximum level of productivity.
Here are 10 tips for establishing secure remote access to a control system. Consult your automation suppliers to fully understand the intrinsic security of your system.
1. Remote Access Should be Granted For Machine Service, But Segregated From the Plant Network
OEMs should only reach the machines under their responsibility in the plant. To achieve this, the system must be configurable to segregate the machine network from the rest of the network. Once completed, the machine network nodes aren’t directly connected to the site network and must be configured with different IP addresses.
2. Separate VPN Access from Machine Control to Verify Performance In Event of a Cybersecurity Incident
Using machine control equipment, such as a PC, HMI or PLC, as a VPN host may reduce its resources and degrade performance. To achieve the control system’s availability, it must provide the resources to operate in a degraded mode during a denial-of-service (DoS) event.
An external router will act as boundary to filter certain types of packets to protect control systems from being directly affected by DoS events, thus avoiding any external attack affecting the control system and stopping the machine.