By Manish Jain, Product Leader for Edge Analytics and AI Applications, and Achim Thomsen, Director of Common Connected Applications, Rockwell Automation
The 2023 MLC Data Mastery and Analytics survey found that more than one-third of manufacturers say the volume of data they’re collecting has at least doubled in the last two years, and nearly 20% say the amount of data has at least tripled. While this data surge presents opportunities for manufacturers, it also presents a critical question: where should manufacturers process and analyze this constantly increasing volume of information?
Enter cloud and edge computing, two distinct approaches to data processing in industrial data management. Cloud computing, with its centralized servers and vast storage capacity, offers scalability and accessibility. On the other hand, edge computing brings processing power closer to the data source, supporting real-time decision-making and low latency.
Both cloud and edge computing have advantages and limitations. Understanding these nuances is imperative for manufacturers to make the right decision that aligns with their unique digitization goals.
The Cloud Advantages
Cloud computing has revolutionized data management by shifting away from on-premises infrastructure. This computing paradigm allows manufacturers to transmit vast amounts of industrial data to IT and operational technology (OT) applications through an Internet connection, unlocking a range of benefits:
- Scalability: Cloud computing offers significant flexibility to adapt to dynamic business needs. This allows manufacturers to easily adjust computing resources based on demand fluctuations, such as varying workloads or evolving data-processing demands. Whether experiencing a sudden surge in data processing needs or periods of reduced activity, cloud platforms provide the agility to optimize costs and maintain operational efficiency.
- Cost-Effectiveness: One advantage is that outsourcing software and infrastructure management to cloud providers reduces the need for dedicated IT personnel and costly hardware. This cuts costs and simplifies operations.
- Accessibility: Cloud computing enhances accessibility by supporting seamless data access and collaboration from any location with an Internet connection. Teams can work collaboratively and access data in real time, irrespective of geographic boundaries. Facilitating remote work empowers employees to be productive and make informed decisions.