By Meghna Subramani, Commercial Product Manager, Network & Cybersecurity, and Andreu Cuartiella, Lifecycle Services Commercial Manager EMEA, Rockwell Automation
The European market for operational technology (OT) is growing at a rate of 7% a year and will be worth US$9 billion by 2028, according to a study from Data Bridge Market Research. Across Europe, manufacturers and operators of infrastructure have invested in connected devices and services. Bringing networked intelligence to the factory floor like this can help increase productivity by the equivalent of an extra $1 per square meter (m3) per day.
Now it’s time to protect that investment — and the need to do is increasingly urgent. In December 2022, the European Union (EU) Commission published the revised Network and Information Systems Directive (Directive (EU) 2022/2555), commonly known as NIS2.
The directive is a legislative act that aims to achieve a high, common level of cybersecurity across the EU. It focuses on a risk-based approach to security, covering areas such as business continuity and crisis management, vulnerability handling and disclosure, and multifactor authentication.
Prepare Your Cybersecurity Posture for NIS2
Even if your facilities were already covered by, and compliant with, the original NIS directive of 2016, you need to pay attention to NIS2, because it introduces some important changes. Some issues that are new in NIS2 include the following:
- The directive applies to new sectors not covered by the original NIS directive, such as water, waste management, critical manufacturing and more.
- Any entity that falls under NIS2 must have risk-analyzed its cybersecurity posture, then developed and documented security processes and incident-handling procedures.
- The supply chain is now covered, so affected entities must assess the cybersecurity of their supply chain and create appropriate risk-management measures.
- Incident-notification rules are much stricter. Entities must notify authorities of a suspected malicious act affecting their IT or OT networks within 24 hours.