Loading
Magazine | Oil & Gas
Recent ActivityRecent Activity
4 minute read

How to Select Edge Technology for Oil & Gas Operations

Follow these tips for choosing the right edge device to help optimize real-time control, improve analytics and secure operations.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
oil pump on blue digital technology background

We’re in the era of high-performance, intelligent electronic devices known as the edge. These ready-to-be-installed technologies perform advanced and sophisticated autonomous operations. The availability of edge solutions is ripe; many manufacturers and suppliers now include edge devices as a standard offering.

For the oil and gas industry, edge computing can provide real-time surveillance, control, automation, complex analytics and autonomy right at the wellbore, alongside production surface equipment, across long hydrocarbon pipelines, and in carbon capture injection wells, among other uses.

But the choices are immense. Major computer manufacturers are even offering advanced field computers as hardware ready to be programmed and installed on site.

Given this, a question arises: How do you select the appropriate edge device that best aligns with your requirements, budget and long-term vision?

Making the Choice Clearer

To make the selection process easier for you, here is a set of capabilities and features an edge device should comply with to be successful.

Hardware and Software: An edge device should offer a symbiotic combination of hardware and software, closely interlaced in providing a functional, safe and robust solution. Obtaining only hardware, selecting an operating system, and then building applications from there may be a long, tortuous and expensive process that requires resources and time.

Robust Hardware: Make sure the edge hardware you select can operate in harsh environments and over a wide operating range.

Keep up with oil, gas & chemical automation trends and technologies
oil rig in the Gulf of Mexico
Subscribe to The Journal
Keep up with oil, gas & chemical automation trends and technologies

Subscribe to The JOURNAL from Rockwell Automation and Our PartnerNetwork’s digital magazine, and receive the oil, gas and chemical industry’s latest news and information directly to your inbox. Enter your email address and check the box for "The Journal." It's that easy!

Subscribe Now

Classic Process Controls, Advanced Analytics and Autonomy in a Single Device: Most edge offerings aren’t designed for real-time, deterministic control. Often, they rely on a separate PLC alongside the edge device.

For the best performance, look for a device that provides PLC IEC 61131 programming capabilities for fine-grained real-time surveillance and control, combined with analytical applications, and built using high-level languages integrated with the PLC engine.

Also, the real-time engine must be physically and logically detached from advanced applications, so if one component fails, the other continues to operate uninterrupted.

On-Board I/O: It should include I/O points: discrete, analog and control, including a few high-frequency scan rate I/O, suited for specific advanced applications.

Hardware Expandability: This includes external I/O — through remote I/O modules — and more data storage, using SD cards, for example.

Software Immutability: It should guarantee that critical software components — operating systems, drivers, libraries, applications — are protected and can’t be tampered with or modified.

Software Modularity: Software architecture should be highly modular, comprised of loosely coupled modules or containers that can be independently replaced or updated.

High Processing Capacity: Any edge device should provide enough computing power to run several advanced applications. It should be built around major programming frameworks and languages and accept add-on hardware co-processor modules, such as graphic processing units (GPUs) and tensor processing units (TPUs).

 Dawn over a petroleum oil pump in Texas.
eHandbook
2024 Oil & Gas Automation

In the "2024 Oil & Gas Automation" eHandbook, learn how an ultrasonic flowmeter can improve process efficiency, how oil field gas flares can become added income and how standardized controls helped expand renewable natural gas infrastructure. Also learn how to better secure operational technology and more.

Published by The Journal From Rockwell Automation and Our PartnerNetwork™ magazine.

Download Now

Seamless Connectivity: Critical to usability, it will include several serial and network ports and wireless communication capabilities such as cellular (LTE/5G), wi-fi, and wireless I/O (LoRa, WirelessHART, others). Ideally, this kind of connectivity will be readily available to any application running on the edge device.

Major Communication Protocols: De facto standard protocols — both server and client — should be available, such as Modbus, OPC/UA and Ethernet/IP™.

Embedded User Visualization Capabilities: For plug-and-play capability, a quality edge device will be use- interface ready if local visualization is required using inexpensive screen hardware.

Remote Management: Edge devices securely configured from a remote site will give ultimate flexibility — including edge management, updates, patches, or new containerized applications — without interfering with ongoing edge operations.

Embedded Cybersecurity: For remote management, and in general, data security is paramount. Any operation inside the device or in any interaction with external systems must adhere to all principal cybersecurity standards and fully adopt Zero Trust Architecture (ZTA).

Accessible and Customizable Coding Capabilities: Finally, building and deploying your applications without intervention or effort from equipment suppliers will give you total flexibility. A software development kit (SDK) means anyone can build applications for deployment.

Make sure developers can use the full extent of existing advanced languages, software frameworks and complex libraries. This allows them to create new programs that can run in real time along with the rest of the edge components.

Your Unique Needs

This list isn’t exhaustive, but we’ve covered many essential considerations. The key takeaway is flexibility. With each operation comes nuanced demands, and you’ll need an edge controller that works with you.

There is a lot to consider. Getting it right will optimize performance, reliability and security now and into the future. While the market offers a range of options, choosing a device that meets the capabilities and features we’ve discussed will provide a valuable platform for moving your operation to the next level.

 

Like this article? Sign up for the digital magazine (4X/year) and e-newsletter from The Journal From Rockwell Automation and Our PartnerNetwork.

 

 

 

The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Endeavor Business Media.

Topics: The Journal Oil & Gas
Recommended for You
Loading
End of An Era: Celebrating The Journal’s 32-Year Legacy
End of An Era: Celebrating The Journal’s 32-Year Legacy
Magazine
Magazine
End of An Era: Celebrating The Journal’s 32-Year Legacy
In our final issue, we bid fond farewell and look at how we started, how we evolved with the industry, and the partnerships that were key to our success.
Viewpoint: I’m What I Wanted to Be When I Grew Up
Viewpoint: I’m What I Wanted to Be When I Grew Up
Magazine
Magazine
Viewpoint: I’m What I Wanted to Be When I Grew Up
Executive Editor Theresa Houck bids a warm farewell as The Journal ceases publication after 32 years.
eHandbook Shares O&G Automation Best Practices
eHandbook Shares O&G Automation Best Practices
Magazine
Magazine
eHandbook Shares O&G Automation Best Practices
This eHandbook shows how oil & gas firms are using digital tools to boost safety, efficiency, data visibility, and compliance across operations.
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left The Journal Chevron RightChevron Right
  5. Chevron LeftChevron Left How to Select Edge Technology for Oil & Gas Operations Chevron RightChevron Right