Configure alarm properties

Configure alarm properties

Configure alarm properties to alert you when the device exceeds configured high or low limits.
To configure alarm properties
  1. On the tab for the device, expand
    Channels
    , and then expand an individual channel.
  2. Select
    Alarms
    .
  3. In the
    Alarms
    view, fill in the parameters and select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal