Configure individual input channel properties

Configure individual input channel properties

Configure the properties of the individual input channel to define the scaling and filtering for that channel.
To configure individual input channel properties
  1. On the tab for the device, expand
    Channels
    , and then select an individual channel.
  2. In the
    Ch0x
    view, fill in the parameters and select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal