View individual event properties

View individual event properties

Use the
Events
view to view event properties for the devices.
To view individual event properties
  1. On the tab for the device, expand
    Events
    , and then select the extended event.
  2. In the
    Event0x
    view, view the parameters for the events.
    TIP:
    To configure event properties, navigate to the
    Tag
    editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.