Configure limit properties

Configure limit properties

Configure limit properties to manage the amount of data coming from an output.
To configure limit properties
  1. On the tab for the device, expand
    Channels
    , and then expand an individual channel.
  2. In the
    Limits
    view, fill in the parameters and select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal