Configure system power alarm properties

Configure system power alarm properties

Configure the alarm properties to trigger the system power alarms when system power exceeds high or low voltage limits.
To configure system power alarm properties
  1. On the tab for the device, select
    Alarms
    .
  2. In the
    Alarms
    view, select
    Enable System Power Alarms
    if it is not already selected to enable the system power alarms.
  3. In the
    High System Power Alarm Limit
    box, enter the maximum voltage allowed before the high system power alarm transitions from off to on.
  4. In the
    Low System Power Alarm Limit
    box, enter the minimum voltage allowed before the low system power alarm transitions from off to on.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal