Bumpy Confirmation dialog box
The connection to the device is disabled due to a change in the:
- Requested Packet Interval (RPI)
- Electronic Keying
- Minor Revision
- Device Definition
- Device Configuration
- Inhibit the device Connection
- Input Type
- Input Trigger
Apply the change:
- SelectYes. The device connection is interrupted to apply the change. If the Inhibit option is selected, the connection is inhibited.
- SelectNoto return to the previous editing session (any profile changes are pending).
Provide Feedback