Calibration mismatch

Calibration mismatch

Performing calibration has the potential to cause unexpected results if:
  • At least one channel is selected, and
  • There is a mismatch between the device in the application's I/O configuration and the actual physical device, and
  • The system is active.
Select
Cancel
to stop the calibration process. Check the configuration, and shut down the system before performing the calibration.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.