Calibration view parameters

Calibration view parameters

Use the
Calibration
view to calibrate the analog devices. The device needs to be inhibited before performing calibration. The
Calibration
view includes these parameters:
TIP:
The parameters cannot be edited when there is a transition to Run mode.
Parameter
Description
Channel
Indicates the number of the channels that are available to be calibrated.
Calibration Range
Shows the range in which the channel is calibrated based on the device and the selected input or output type.
Calibration Gain
Shows the calibration gain as reported by the device.
Calibration Offset
Shows the signed values as reported by the device.
Last Calibration Date
Shows the date that the device was last successfully calibrated.
Calibration Status
Shows the status of the calibration per channel as the calibration occurs.
Start Calibration
Opens
Calibration Wizard
and starts the calibration process.
Start Calibration
is enabled when the device is inhibited, online with the controller, and at least one channel is selected to start the calibration process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.