Input device calibration parameters

Input device calibration parameters

The
Select Channels to Calibrate
view applies to the 1756-IF8I and 1756-IRT8I devices. These parameters are available in this view.
TIP:
The parameters cannot be edited when there is a transition to Run mode.
Parameter
Description
Channel
Shows the channels available to calibrate.
Calibrate
Select to calibrate the channel.
Calibration Range
Shows the calibration range currently configured for channel.
The range depends on the
Input Type
selection.
Calibration Gain
Shows the calibration gain reported by the device.
Calibration Offset
Shows the signed value as reported by the device.
Calibration Status
Shows the status of the calibration as the calibration occurs.
Calibrate channels in groups
Select to apply a reference signal to all of the selected channels at the same time.
Calibrate channels one at a time
Select to apply a reference signal to one channel and then move the reference to the next channel.
If check box is selected, the selected channels are calibrated one at a time.
Next
Starts the calibration of the channel.
If the value for the channel is acceptable, and another channel is selected to be calibrated, the next channel is highlighted. Select
Next
to calibrate the next channel.
Retry
Restarts the calibration for the channel.
Stop
Stops the calibration process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.