Output Reference Signals - High Reference (mA)

Output Reference Signals - High Reference (mA)

The output device starts to send high reference signals on all the selected current channels. This window opens after the successful calibration of voltage channels (if any). These parameters are available in
Output Reference Signals - High Reference (mA)
.
Parameter
Description
Channel
Shows the channels available to calibrate.
Calibrate
Identifies the channels selected in the previous window.
Calibration Range
Shows the
High Reference Signal
value that the device produces based on channel configuration. The calibration range shows 0 mA to 20 mA for Current.
High Reference
Shows the
High Reference Signal
value that the device produces on the channel. For current channels, the value is 20 mA.
Back
Returns to the previous wizard window.
Next
Starts producing the reference signal on the selected channels.
Stop
Stops the calibration process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.