Output Reference Signals - High Reference (Volts)
The output device starts to send high reference signals on all the selected voltage channels. These parameters are available in
Output Reference Signals - High Reference (Volts)
.Parameter | Description |
---|---|
Channel | Shows the channels available to calibrate. |
Calibrate | Identifies the channels selected in the previous window. |
Calibration Range | Shows the High Reference Signal value that the device produces based on channel configuration. The calibration range shows -10 V to 10 V for Voltage. |
High Reference | Shows the High Reference Signal value that the device produces. For voltage channels, the value is 10 V. |
Back | Returns to the previous wizard window. |
Next | Starts producing the reference signal on the selected channels. |
Stop | Stops the calibration process. |
Provide Feedback