Results - Low Reference Signals

Results - Low Reference Signals

The device reads the value for the enabled channels.
  • If the reference signal is within the acceptable range, the status shows
    OK
    for that channel. Select
    Next
    to go on to the High Reference Test.
  • If the reference signal is not within the acceptable range, the status shows
    Error
    for that channel. Investigate the channels with errors, and then select
    Retry
    to perform calibration again on channels with errors.
You can also select
Cancel
and exit
Calibration Wizard
leaving the calibration status for that channel with an Error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.